154 Topic(s)
Use the Xenta Schedule workspace to navigate, add, remove, or edit events.
System displays the entire tree structure of Building Operation as it appears in WorkStation.
Custom View lists the objects and functions that are available in the Custom View folder of Building Operation in a logical manner, such as hierarchical, geographical, or functional. So, you do not see the entire tree structure of WorkStation, just the parts that you want to see or all the parts in the order that you want. For example, in WorkStation, you create a Custom View that contains variables of a Campus that you want to monitor from Technician Tool.
You edit the end time for a schedule event to make the event end at another point of time in the schedule. You can edit the end time for weekly events as well as exception events.
You view schedule events to see the schedule for one or more events.
You scroll a month in a calendar using the next and prev buttons.
You scroll a month in a schedule using the Forward and Backward buttons.
You scroll a week in a schedule using the Forward and Backward buttons.
You scroll a day in a schedule using the Forward and Backward buttons.