Schedules

153 Topic(s)
Use the filters below to limit the number of search hits.
Products
Information Type
Topic
Modified
Rating
Setting the Time Increments in the Server Time Bar
You set the time increments in the Server Time bar to adjust the time value bars in the Graphic View.
3/4/2019
Schedule Navigation in WorkStation
You have some navigation tools to use when you navigate the Basic Schedule Editor, the Advanced Schedule Editor, and the Calendar Editor. To navigate the editors, you can use the tools described in the following table.
5/18/2018
Custom View
Custom View lists the objects and functions that are available in the Custom View folder of Building Operation in a logical manner, such as hierarchical, geographical, or functional. So, you do not see the entire tree structure of WorkStation, just the parts that you want to see or all the parts in the order that you want. For example, in WorkStation, you create a Custom View that contains variables of a Campus that you want to monitor from Technician Tool.
5/14/2018
System
System displays the entire tree structure of Building Operation as it appears in WorkStation.
5/14/2018
Schedule Event Properties Dialog Box – Calendar Reference View
Use the Calendar Reference view in the Schedule Event Properties dialog box to reference a calendar to apply to your schedule.
2/26/2018
Schedule Event Properties Dialog Box – Calculated Exception View
Use the Calculated Exception view in the Schedule Event Properties dialog box to schedule recurring exceptions.
2/26/2018
Schedule Event Properties Dialog Box – Single Date Exception View
Use the Single Date Exception view in the Schedule Event Properties dialog box to schedule a single date exception.
2/26/2018
Schedule Event Properties Dialog Box – Date Range Exception View
Use the Date Range Exception view in the Schedule Event Properties dialog box to schedule a date range exception.
2/26/2018
Schedule Event Properties Dialog Box – Weekly View
Use the Weekly View in the Schedule Event Properties dialog box in the Basic Schedule Editor to create a new weekly event for an existing schedule.
2/26/2018
Xenta Schedule Workspace
Use the Xenta Schedule workspace to navigate, add, remove, or edit events.
2/12/2018

Product version

Language