195 Topic(s)
An exception event occurs instead of the scheduled weekly events for a single date, date range, calculated date, or calendar reference.
Use the Schedule workspace to navigate, add, remove, or edit events.
A schedule has a color code so you can identify weekly events and exception events at a glance. This color code can assist you when you are modifying your schedule or trying to troubleshoot any problems.
You use the Schedule Workspace Toolbar to edit the selected schedule.
You can create a Multi schedule viewer in WebStation to edit and view a number of schedules at the same time.
A calendar is a list of dates. The calendar provides the schedule with the dates when the exception events shall occur. To save time, you can reference a single calendar rather than entering several exception events in a schedule.
You specify a single date in a calendar. A date is an entry that occurs once in the calendar.
A weekly event occurs every week for an extended period of time on a regular basis. You can schedule more than one weekly event for each day of the week.
You view schedule events to see the schedule for one or more events.
You use the Calendar Editor to specify dates of exception events in a calendar. You can add and remove single dates. By using a calendar, you specify all the exception events only one time, rather than in each schedule. The calendar is then referenced to each of the schedules and all exception dates are automatically designated in the schedules.