earth_america
user_standard Log on
action_search_stroke
earth_america

SpaceLogic Sensor Interfaces

Touchscreen
LCD
3-button
Refine your search
arrow2_down
Refine your search

37 Topic(s)

How to

In the SpaceLogic Sensor Touchscreen Display model, you change the occupancy mode to tell the control system that the room is occupied or unoccupied. You do so by enabling the Display object Occupancy override property. Depending on the control system programming, it may respond in various ways including changing the active setpoint from unoccupied to occupied, turning on the lights, and/or starting a timer that expires when the system becomes unoccupied again.

Concept

When the room occupant presses the buttons on the SpaceLogic Sensor 3-Button Cover model to increase or decrease the temperature setpoint, the backlight changes from deep blue at the low end of the range, to deep red at the top end of the range. Each button push causes a 10% increase or decrease in the range. The backlight flashes rapidly three time to indicate the top or bottom of range has been reached.

Concept

The 3-Button Cover model contains a passive, infrared sensor for occupancy detection and a plus and minus button to adjust the temperature setpoint. There is also an occupancy override button should the room occupant wish to confirm their presence, turn on the lights, and change the setpoint to a comfortable level.

Concept

The Touchscreen Display model provides a menu-driven interface with a front menu and a functions menu screen that you configure through EcoStruxure Building Operation.

Concept

SpaceLogic Sensor devices are modular and are ordered in two parts: the sensor base and the cover. Four SpaceLogic communicating sensor base models are available as well as a variety of covers.

Concept

SpaceLogic Sensors are a family of living space sensors designed for BACnet/IP controllers using the EcoStruxure Building Operation user interface. These sensors use an RJ-45 sensor bus that provides communication and power from the BACnet/IP controller.

How to

In the SpaceLogic Sensor 3-Button Cover model, you override the living space occupancy setting, for example, so an after-hours occupant can change the control setting to improve their comfort level. You enable occupancy override and also use the current occupancy value to control applications using the Display object Occupancy override property.

How to

In the SpaceLogic Sensor Touchscreen Display model, you select the degree type in order to see the temperature in the preferred units of the room occupant. You enable this feature by choosing the Display object Allow temperature unit changes property, followed by the Temperature units property and its Fahrenheit or Celsius option.

How to

In the SpaceLogic Sensor Touchscreen model, you select the fan speed to change the air flow in the designated living space. You enable this feature using the Display object Allow fan speed changes property.

How to

You can program lighting control to create special scenes that illuminate an area based on the time of day, such as dimming the lights with the click of the night light button.