Trends

247 Topic(s)
Use the filters below to limit the number of search hits.
Products
Information Type
Topic
Modified
Rating
Trend Log Lists in WorkStation
A trend log list displays all values in the trend log in a list.
12/20/2018
Trend Log List Context Menu
Right-click a row in a trend log list to open the trend log list context menu, where you can edit a record, show the history of a record, or copy the trend log list data.
12/20/2018
Custom View
Custom View lists the objects and functions that are available in the Custom View folder of Building Operation in a logical manner, such as hierarchical, geographical, or functional. So, you do not see the entire tree structure of WorkStation, just the parts that you want to see or all the parts in the order that you want. For example, in WorkStation, you create a Custom View that contains variables of a Campus that you want to monitor from Technician Tool.
5/14/2018
System
System displays the entire tree structure of Building Operation as it appears in WorkStation.
5/14/2018
Context Menu – Open Chart Submenu
Use the Open chart submenu to create a new chart.
2/2/2018
Saving Current Trend Chart Settings
You save the trend chart settings if you want the trend chart to be displayed the same way the next time you open it.
1/30/2018
Viewing the Value Closest to the Pointer
Use the Magnetic function to view the value closest to the pointer.
1/29/2018
Temporary Trend Charts
​To display a trend log without creating a new trend log list or trend chart, the trend log can be displayed in a temporary list or chart.
10/12/2017
Temporary Trend Log Lists
​To display a trend log without creating a new trend log list or trend chart, the trend log can be displayed in a temporary list or chart.
10/12/2017
Trend Chart Axes
The x-axis of the trend chart represents time. The time span of the axis can be set with a fixed start and end time or with an end time relative to the present time. The axis can be quick-scaled to show the last hour, last day, last month, or last year​.
10/12/2017

Product version

Language