earth_america
user_standard Log on
action_search_stroke
earth_america

Trends

Refine your search
arrow2_down
Refine your search
Ok
Ok
Ok

279 Topic(s)

Specifications

How to

You enable the TimescaleDB connection for all servers that are supposed to have a connection to the database.

Concept

You use an extended trend log to store records from a trend log. An extended trend log can be connected to a trend log or connected in a series to another extended trend log. Only one extended trend log can be connected to a trend log​ or another extended trend log.

Concept

A log processing trend log enables calculation within or between various trend logs. With this feature, building managers can gather new information about how the building is operating, they can view historical data that is calculated against new data and in this way detect new trends, they can compare various values and calculate a new trend log displaying relativised behavior, or unify measurements made with different units. The results from these calculations can indicate anomalies that have other reasons than the naturally varying conditions, so that it becomes easier to find problems with the building.

Concept

The function of a trend log is to log the variable that it is connected to and store the records.

How to

You open diagnostics in WebStation to check the health of your system.

Concept

You use a trend log to collect data and then store the records. A record contains a log value or an event as well as its time stamp and an optional comment. A trend log can log an analog variable, a digital variable, or an integer variable.

Concept

You use trend logs to record values, such as a sensor. A trend log can also log consumptions, such as energy consumption or water consumption.

How to

You disable the TimescaleDB connection for all servers that are supposed to have a connection to the database you are backing up and/or restoring to make sure you are working with the correct database.

Concept

​The implicit log is a change of value trend log which monitors the IO variable and records a new value if the variable exceeds the delta. Each log value is stored as a record in the trend log. The delta is automatically defined by the EcoStruxure Building Operation software depending on the measured unit of the device that is connected to the IO port.