9 Topic(s)
The installer is used for both maintenance release upgrades and hotfix installations on Enterprise Central and Enterprise Server.
Use this workflow to change the operating system on the computer where the Enterprise Server is installed. You can also use this workflow to migrate WebReports or the Enterprise Server to another computer.
Use the Operator Display Settings screen to configure Operator Display and perform administrative tasks.
Use the Choose Components page to define which products to install.
Use the Firmware Update screen to upload a new version of the firmware to the Operator Display.
You upgrade the firmware to access the latest Operator Display features and bug fixes.
Use the Installation Type page to define which type of installation to perform when corresponding product is already installed on your computer or server.
Use the License Server Configuration page to configure the address to the license server.
Use the Configuration page to configure the port number the Enterprise Server listens to when communicating through a specific protocol.