189 Topic(s)
You set an EcoStruxure BMS server to password reset mode so that you can create a new password if the old one was forgotten.
Use the User Account Group properties dialog box to configure the properties of a user account group.
You can map Windows Active Directory groups to EcoStruxure Building Operation user account groups if the EcoStruxure Building Operation software runs on a network that uses this directory to manage users and user account groups. An EcoStruxure Building Operation user account group that includes a Windows account group can be member of another EcoStruxure Building Operation user account group.
You create a domain to group EcoStruxure BMS servers, users, and user groups in one domain so that all users and user groups of the domain have access to all EcoStruxure BMS servers within the domain. You can connect the domain to a Windows Active Directory domain to make user accounts from the Windows Active Directory accessible to the EcoStruxure Building Operation software, and to allow users to log on to WorkStation with their Windows user account. You cannot directly add an automation server to a domain in an Enterprise Central.
Use the Domain Members page to add an automation server to the domain.
An EcoStruxure Building Operation domain contains user accounts, user account groups, software permissions, workspaces, and one or several EcoStruxure BMS servers. The EcoStruxure BMS server that hosts and administers the domain is called the domain controller.
You assign an automation server to a domain in the live system to extend your current domain.
You configure user settings to configure the setttings for all users on this Operator Display.
Use the Create password for screen to assign a unique password to the new user.
Use the Create User screen to create a new user account on this Operator Display.