194 Topic(s)
Use the Policies tab to edit the policy settings for a user account group.
Use the Operator Display Settings screen to configure Operator Display and perform administrative tasks.
SpaceLogic* Operator Display is a touch-screen Human Machine Interface (HMI) for SpaceLogic controllers and servers, designed for local monitoring of building controllers in small and medium-sized buildings, as well as in large buildings with comprehensive building management systems. Operator Display is specifically designed for equipment rooms and it simplifies operations, service, and troubleshooting for System Integrators and Service Engineers, as well as for non-technical users (notably Facility Managers and Janitors).
When logging on to an EcoStruxure BMS server, you have to authenticate yourself by using a valid user account. The user account has to belong to the same domain as the server you log on to.
You set an EcoStruxure BMS server to password reset mode so that you can create a new password if the old one was forgotten.
You can reset the administrator password on your EcoStruxure Building Operation servers. Related information can be found in the sections after the flowchart.
You prevent a group of users from exiting WorkStation to make sure that WorkStation is not closed on a permanent EcoStruxure BMS computer. This feature must be disabled for all user account groups the user is a member of.
Use the Profile tab to edit the information about the user the account belongs to.
You review the workspace memberships for a user account group to determine if the user account group, for example, needs additional workspaces.
The automatic logoff function makes it possible for the system to automatically log off a user after a specified time of inactivity.