How to

721 Topic(s)
Use the filters below to limit the number of search hits.
Products
Functionality
Topic
Modified
Rating
Rechecking Alarms
You recheck alarms to refresh the information in the Alarms pane.
8/16/2019
Wiring a Terminal Block
You wire the terminal blocks installed on the AS-B to connect I/O devices, RS-485 network devices, and power.
5/22/2019
Wiring a Terminal Base
You can wire a terminal base prior to installing an electronics module.
5/22/2019
Connecting AD to AS-P or AS-B
You connect AD to an AS-P or AS-B in order to communicate with SmartStruxure servers over a USB connection, to supply the AD with power, and to ensure that its battery is charged.
5/21/2019
Installing the AD v1 Tablet and Frame
You install the AD v1 tablet and the frame on the base to install AD v1 on a control cabinet or a wall and to provide the tablet with a protective frame.
5/21/2019
Powering Up an AS-B
You perform the following steps to power up an AS-B.
5/20/2019
Installing AS-B on a DIN Rail
You install AS-B on a horizontal DIN rail to ensure that the device is securely fastened and to allow sufficient cooling air flow through the device.
5/20/2019
Installing a Terminal Base on a DIN-rail
You install a terminal base on a horizontal DIN-rail prior to connecting it to its neighboring terminal bases.
5/20/2019
Connecting AD to Automation Server and a Power Adapter
You connect AD to an Automation Server in order to communicate with SmartStruxure servers over the USB connection. You connect AD to a USB power adapter in order to supply AD with power and to ensure that its battery is charged. You use a USB “Y” cable to connect AD to both an Automation Server and a USB power adapter.
5/19/2019
Removing a Terminal Block
You remove a terminal block from AS-B to replace the device.
5/19/2019

Product version

Language