How to

721 Topic(s)
Use the filters below to limit the number of search hits.
Products
Functionality
Topic
Modified
Rating
Wiring a Terminal Block
You wire the terminal blocks installed on the AS-B to connect I/O devices, RS-485 network devices, and power.
5/22/2019
Wiring a Terminal Base
You can wire a terminal base prior to installing an electronics module.
5/22/2019
Connecting AD to AS-P or AS-B
You connect AD to an AS-P or AS-B in order to communicate with SmartStruxure servers over a USB connection, to supply the AD with power, and to ensure that its battery is charged.
5/21/2019
Installing the AD v1 Tablet and Frame
You install the AD v1 tablet and the frame on the base to install AD v1 on a control cabinet or a wall and to provide the tablet with a protective frame.
5/21/2019
Powering Up an AS-B
You perform the following steps to power up an AS-B.
5/20/2019
Installing AS-B on a DIN Rail
You install AS-B on a horizontal DIN rail to ensure that the device is securely fastened and to allow sufficient cooling air flow through the device.
5/20/2019
Installing a Terminal Base on a DIN-rail
You install a terminal base on a horizontal DIN-rail prior to connecting it to its neighboring terminal bases.
5/20/2019
Connecting AD to Automation Server and a Power Adapter
You connect AD to an Automation Server in order to communicate with SmartStruxure servers over the USB connection. You connect AD to a USB power adapter in order to supply AD with power and to ensure that its battery is charged. You use a USB “Y” cable to connect AD to both an Automation Server and a USB power adapter.
5/19/2019
Removing a Terminal Block
You remove a terminal block from AS-B to replace the device.
5/19/2019
Installing a Terminal Block
You install the terminal blocks on AS-B to add or enable wiring for the device.
5/19/2019

Product version

Language