earth_america
user_standard Log on
action_search_stroke
earth_america

How to

Refine your search
arrow2_down
Refine your search
Ok
Ok
Ok

1070 Topic(s)

How to

You can wire a terminal base prior to installing an electronics module.

How to

You print an I/O wiring list for the I/O bus that describes which I/O points are associated with each I/O module. You use the printed copy of this list to help wire the I/O bus network.

How to

You print labels to identify I/O channels on the placard of an I/O module much the same way you label circuits on an electrical panel. You accept the default names for the I/O point labels or customize the I/O point names for your own application.

How to

You perform the following steps to power up a device.

How to

You install an electronics module directly onto the relevant terminal base, where it will connect to the power supply and address bus.

How to

You install a terminal base on a horizontal DIN rail to ensure that the device is securely fastened and to allow sufficient cooling air flow through the electronics module. You install a terminal base on a DIN rail prior to connecting it to its neighboring terminal bases.

How to

You connect terminal bases together to provide continuity of the power supply and the address bus.

How to

You connect a Central IO module terminal base to an AS-P-3 server to supply power to the Central IO module, give the module an address, and communicate with the module via the I/O bus.

How to

You connect an air velocity probe installed in the duct inlet to the RP-V onboard air flow sensor (differential velocity pressure sensor) to measure the air flow in the VAV terminal unit.

How to

You install the RP-V directly over the VAV damper shaft for damper positioning control and air flow sensing. When you install the RP-V on a damper that rotates counter-clockwise (CCW) to open, use WorkStation or the Commission mobile application to ensure that the configured direction of the actuator rotation matches the damper type.