1073 Topic(s)
You clear the list of the display names and IP addresses of servers when you do not need the contents anymore.
You configure an automation server to use 802.1X Protected EAP to increase the security.
You configure a log gauge to display a trend log in a gauge.
You configure an automation server to use 802.1X EAP TLS to increase the security.
You configure an automation server to use 802.1X MD5 to increase the security.
You log on to WorkStation to securely access the functions in the EcoStruxure BMS.
You edit a backup rule on an EcoStruxure BMS server to change the type of data that you want to back up. You can also set up this backup rule to follow a shadow schedule that references a lead schedule managed on another EcoStruxure BMS server.
You create an out of reference range alarm to trigger an alarm when a variable, such as a temperature, differs from a reference value.
You create an out of range alarm to trigger an alarm when a variable, such as a temperature, is not within its specified range.
You connect RP controller expansion modules and multi-sensors to the RP-C room bus to provide the devices with power and communication from the RP-C controller.