earth_america
user_standard Log on
action_search_stroke
earth_america

AD v3

Refine your search
arrow2_down
Refine your search
Ok
Ok
Ok

14 Topic(s)

Hardware Installation

Hardware Installation

Concept

The Schneider Electric SpaceLogic hardware devices for the EcoStruxure BMS include terminal bases, PS-24V power supplies, Central IO modules, automation servers such as AS-P servers and AS-B servers, BACnet/IP devices such as MP-C controllers, MP-V controllers, IP-IO modules, and RP-C controllers, RP controller expansion modules, remote control, KNX Modbus gateway, Bluetooth adapter, Wireless Adapter - Advanced, SpaceLogic Sensor devices, Advanced Display devices, and Operator Display devices.

Specifications

Concept

Advanced Display v3 (AD v3) is the successor to AD v2. AD v3 provides an industrial grade Human Machine Interface (HMI), with battery-free power supply, for local access to the EcoStruxure BMS servers.

How to

You connect AD v3 to an automation server in order to communicate with the automation server over a wired (USB) connection. You connect AD v3 to a 24 VDC power supply in order to supply AD v3 with power. You use the Y-shaped cable (SXWADUSBC10002 or SXWADUSBC10003) to connect AD v3 to both the automation server and the power supply.

Specifications

Concept

AD v3 uses a wired (USB) connection to communicate with automation servers and the device must be powered by a 24 VDC power supply.

How to

You install AD v3 on a control cabinet to use AD v3 for locally accessing the automation servers.

Concept

AD v3 has a power button that is used to power on the device, to turn off or reboot the device, and to perform other actions.