15 Topic(s)
The Schneider Electric EasyLogic and SpaceLogic hardware devices for the EcoStruxure BMS include terminal bases, PS-24V power supplies, Central IO modules, automation servers such as AS-P-3, AS-P and AS-B servers, MP-C, MP-V, RP-C, and RP-V controllers, IP-IO and RP-IO I/O modules, RP controller expansion modules, remote control, KNX Modbus gateway, Bluetooth adapter, Wireless Adapter - Advanced, SpaceLogic Sensor devices, Advanced Display devices, and Operator Display devices.
This section provides information on regulatory and agency compliance and approvals for the Advanced Display v3 (AD v3).
Part number: SXWADBUND10013
Part number: SXWADWIFI10002
You connect AD v3 to an automation server in order to communicate with the automation server over a wired (USB) connection. You connect AD v3 to a 24 VAC or 24 VDC power supply in order to supply AD v3 with power. You use the Y-shaped cable with USB isolation (SXWADUSBC10012 or SXWADUSBC10013) to connect AD v3 to a 24 VAC power supply. You use either the Y-shaped cable with USB isolation or the Y-shaped cable without USB isolation (SXWADUSBC10002 or SXWADUSBC10003) to connect AD v3 to a 24 VDC power supply.
You replace the CMOS battery in AD v3 to be able to boot up AD v3 when the existing battery is dead.
Advanced Display v3 (AD v3) is the successor to AD v2. AD v3 provides an industrial grade Human Machine Interface (HMI), with battery-free power supply, for local access to the EcoStruxure BMS servers.
This section provides safety information specific to AD v3. Carefully read the instructions before trying to install, operate, service, or maintain the equipment.