1456 Topic(s)
Use the Building Operation WorkStation window to log on to WorkStation.
You use theDisplay Names and IP Addresses of Servers drop-down list box to add, edit and delete the display names of the server addresses. You also use it to export, import and delete lists of the display names and IP addresses of servers.
You configure an automation server to use 802.1X Protected EAP to increase the security.
You configure an automation server to use 802.1X EAP TLS to increase the security.
Automation servers support IEEE 802.1X security. Automation servers can be configured as supplicants on a network protected by IEEE 802.1X security.
You configure an automation server to use 802.1X MD5 to increase the security.
You edit a backup rule on an EcoStruxure BMS server to change the type of data that you want to back up. You can also set up this backup rule to follow a shadow schedule that references a lead schedule managed on another EcoStruxure BMS server.
You create an out of reference range alarm to trigger an alarm when a variable, such as a temperature, differs from a reference value.
You create an out of range alarm to trigger an alarm when a variable, such as a temperature, is not within its specified range.
You create an interval trend log to record a value of a variable at specified and regularly occurring increments of time.