1149 Topic(s)
You edit a backup rule on an EcoStruxure BMS server to change the type of data that you want to back up. You can also set up this backup rule to follow a shadow schedule that references a lead schedule managed on another EcoStruxure BMS server.
You create an out of reference range alarm to trigger an alarm when a variable, such as a temperature, differs from a reference value.
You create an out of range alarm to trigger an alarm when a variable, such as a temperature, is not within its specified range.
You create an interval trend log to record a value of a variable at specified and regularly occurring increments of time.
You create an extended trend log to store log records for a longer period of time and free up memory in the SmartX server. Extended trend logs are also required for generating reports using EcoStruxure Building Operation WebReports.
You create a change of state alarm to trigger an alarm when a variable, such as a switch, is either true or false.
You back up multiple EcoStruxure BMS servers manually to copy and store data that is frequently updated.
The EcoStruxure Building Operation software handles values and numbers with the highest precision. By default, the unit of a value is converted according to the regional settings of the user’s operating system.
By default, WorkStation presents language, date, time, currency, unit, and decimals according to the regional settings of the user’s operating system.
In WorkStation, you add one or more Xenta OP operator panels to the Building Operation network.