BACnet/IP Devices

381 Topic(s)
Use the filters below to limit the number of search hits.
Functionality
Display all
Basic Functionality
Hardware
Central IO
Programming
Trends
Alarms
Schedules
Graphics
Reports
BACnet
LonWorks
Localization
License Management
Engineering
Import/Export
User Management
I/NET
MicroNet
Sigma
MNB
Modbus
Xenta
b3
NETWORK 8000
MNL
Communication Configuration
Web Services
Upgrade
Registration
Vista Transition
Security
Smoke Control
SmartDrivers
Transition
Continuum Transition
Infinet
Custom Types
BACnet/IP devices
3-button
LCD
Touchscreen
SpaceLogic Sensor Interfaces
RP Controller Expansion Modules
Engage Mobile Application
Zoning
RP-C-RC-BLE
KNX
Zigbee
IoT
SE8000/VT8000
Administration
Semantic
Information Type
Display all
Concept
User Interface
Troubleshooting
Developers Reference
Specifications
How to
Hardware Installation
Topic
Modified
Rating
Connecting RP Controller Expansion Modules and Multi-sensors to RP-C
You connect RP controller expansion modules and multi-sensors to the RP-C room bus to provide the devices with power and communication from the RP-C controller.
11/9/2022
RP-C BACnet MS/TP Support
The RP-C controllers can be reconfigured to communicate with automation servers based on the BACnet MS/TP protocol, instead of the BACnet/IP protocol.
11/8/2022
11/2/2022
11/2/2022
Connecting a Non-isolated RS-485 Adapter
You connect a Non-isolated RS-485 Adapter (via a separate connection cable) to a BACnet/IP controller to convert the controller RS-485 RJ45 interface to screw terminals, which is required to connect the controller to a BACnet MS/TP (RS-485) network. You use a Non-isolated RS-485 Adapter (SXWNISORS48510001) when the BACnet MS/TP network includes non-isolated controllers, such as the b3 BACnet family of zone controllers.
10/25/2022
Connecting an Isolated RS-485 Adapter
You connect an Isolated RS-485 Adapter (via a separate connection cable) to a BACnet/IP controller to convert the controller RS-485 RJ45 interface to screw terminals, which is required to connect the controller to a BACnet MS/TP (RS-485) network. You use an Isolated RS-485 Adapter (SXWISORS48510001) when the BACnet MS/TP network is comprised of isolated controllers, such as MNB BACnet devices (zone controllers) and selected others.
10/25/2022
RP-C Sensor Bus
The RP-C sensor bus allows SpaceLogic Sensor devices to be connected to the controller.
10/3/2022
RP-C Communication Ports
The RP-C provides the following combination of communication ports:
10/3/2022
Isolated RS-485 Adapter
The Isolated RS-485 Adapter (SXWISORS48510001) is designed to be used when connecting a BACnet/IP controller that supports reconfiguration for BACnet MS/TP communication to a BACnet MS/TP (RS-485) network. The Isolated RS-485 Adapter has an isolated RS-485 transceiver and is used when the BACnet MS/TP (RS-485) network is comprised of isolated controllers, such as MNB BACnet devices (zone controllers) and selected others.
9/20/2022

Product version

Language