earth_america
user_standard Log on
action_search_stroke
earth_america

BACnet/IP Devices

RP-C
RP-V
MP-C
MP-V
IP-IO
RP-IO
MP-C Smoke Control
MP-V Smoke Control
IP-IO Smoke Control
Refine your search
arrow2_down
Refine your search
Ok
Ok
Ok

504 Topic(s)

Concept

The RP-C-16A model has 16 I/O points and the controller is equipped with 30 fixed screw terminals.

Concept

The RP-C-12C model has 12 I/O points and the controller is equipped with 24 fixed screw terminals.

Concept

The RP-C-12B model has 12 I/O points and the controller is equipped with 24 fixed screw terminals.

Concept

The RP-C-12A model has 12 I/O points and the controller is equipped with 23 fixed screw terminals.

Concept

You must configure the DIP switches as part of the commissioning process for the RP and MP controllers and RP-IO modules that only support BACnet MS/TP communications.

Concept

Concept

Ensuring the EcoStruxure Building Management integration is installed securely is key to the overall security envelope of the building. The following integration security configurations need to be considered to ensure the overall security meets “best practice” standards.

Hardware Installation

Part numbers: SXWMPC15A10A01, SXWMPC18A10A01, SXWMPC18B10A01, SXWMPC24A10A01, and SXWMPC36A10A01

How to

You connect RP controller expansion modules and multi-sensors to the RP-C room bus to provide the devices with power and communication from the RP-C controller.

Concept

The IP-IO module provides I/O expansion to your HVAC application over BACnet/IP and can share their I/O resources across applications running in automation servers, BACnet/IP controllers, or third-party systems. The IP-IO module can be installed near facilities in the field, away from the automation server or the BACnet/IP controller.