505 Topic(s)
The RP-C-16A model has 16 I/O points and the controller is equipped with 30 fixed screw terminals.
The RP-C-12C model has 12 I/O points and the controller is equipped with 24 fixed screw terminals.
The RP-C-12B model has 12 I/O points and the controller is equipped with 24 fixed screw terminals.
The RP-C-12A model has 12 I/O points and the controller is equipped with 23 fixed screw terminals.
You must configure the DIP switches as part of the commissioning process for the RP and MP controllers and RP-IO modules that only support BACnet MS/TP communications.
Ensuring the EcoStruxure Building Management integration is installed securely is key to the overall security envelope of the building. The following integration security configurations need to be considered to ensure the overall security meets “best practice” standards.
Part numbers: SXWMPC15A10A01, SXWMPC18A10A01, SXWMPC18B10A01, SXWMPC24A10A01, and SXWMPC36A10A01
You connect RP controller expansion modules and multi-sensors to the RP-C room bus to provide the devices with power and communication from the RP-C controller.
The IP-IO module provides I/O expansion to your HVAC application over BACnet/IP and can share their I/O resources across applications running in automation servers, BACnet/IP controllers, or third-party systems. The IP-IO module can be installed near facilities in the field, away from the automation server or the BACnet/IP controller.