78 Topic(s)
Input modules support a single electrical type, such as digital or universal inputs. The available second version (v2) input modules include the following:
The second-generation (v2) Central IO modules feature several enhancements over the first-generation models, including faster processor performance and higher-resolution A/D converters for universal inputs. Additionally, the v2 module design has been updated to better align with the DIN 43880 standard by removing the previously high shoulder height. By adding a variety of Central IO and power supply modules, you can use the AS-P server to tailor the Intelligent Building Management System to your unique requirements.
Part numbers: SXWUI16XX10002, SXWUI8D4X10002, SXWUI8D4H10002, SXWUI8A4X10002, SXWUI8A4H10002, SXWUI8V4X10002, SXWUI8V4H10002
Part number: SXWTBIOW110002
This Central IO module is a universal input, 16-channel I/O module. You can use the universal inputs for any mix of temperature, pressure, flow, status points, and similar inputs. You can also make adjustments for various sensor types using the available pull-up resistors.
By adding a variety of I/O and power supply modules, you can use the SmartX AS-P server or Automation Server to tailor the Intelligent Building Management System to your unique requirements.
The UI-16 I/O module is a universal input, 16-channel I/O module. Each channel has a dedicated status two-color LED that provides local monitoring of digital, counter, and supervised input types. The front panel shows the module status LED and the I/O channel status LEDs.
Input modules support a single electrical type, such as digital or universal inputs. The available input modules include the following:
This section outlines the recommended cables and wires, specifying the appropriate wire sizes and lengths for the Central IO modules.