earth_america
user_standard Log on
action_search_stroke
earth_america

Commission

Refine your search
arrow2_down
Refine your search
Ok
Ok
Ok

42 Topic(s)

Concept

These hardening guidelines apply to the EcoStruxure Building Commission mobile application.

Specifications

How to

You can select the Feedback option to rate your experiences and provide detailed information on the Commission mobile application.

Concept

You can choose from several different options to connect the eCommission SmartX Controllers mobile application to one or more SmartX IP controllers.

Concept

Prior to using the eCommission SmartX Controllers mobile application at a job site, there are certain preparations that must be made. Complete the following tasks, as well as any additional tasks that may be necessary.

How to

You launch and then activate the eCommission SmartX Controllers mobile application so that it can be used.

Troubleshooting

You use the Controller List Creator function of the eCommission SmartX Controllers mobile application to scan the tear-off product info label on a SmartX IP controller. In the List Creator view, you note that the captured data appears in red text, indicating that you have duplicated a previous scan. This duplication is also indicated with red text in the originally scanned data set.

How to

When necessary, temporarily unhost a SmartX IP controller from the server to allow a task to be performed or completed.

Concept

You can use the Device Restart function of the eCommission SmartX Controllers mobile application to perform a restart of the SmartX IP controller. Two types of restart are possible, Warm Restart and Cold Restart. Most of the actions performed by these restart types are the same, except one:

Concept

Use this workflow to connect the eCommission SmartX Controllers mobile application to SmartX IP controllers.