earth_america
user_standard Log on
action_search_stroke
earth_america

Device Administrator

Refine your search
arrow2_down
Refine your search

15 Topic(s)

User Interface

Use the Installation Type page to define which type of installation to perform when corresponding product is already installed on your computer or server.

Concept

Concept

Before upgrading the system, it is strongly recommended that you archive the historical data and back up the SmartStruxure servers to preserve the current data and configurations. If you plan to upgrade WebReports, be sure to back up the Reports database in SQL Server.

Concept

Schneider Electric recommends that you install the license server framework before other Building Operation software or SmartStruxure server devices. The license server installation is included in the License Administrator license package. During the installation of WorkStation or Enterprise Server, the installation software asks for the address to the license server.

Concept

The Building Operation products are installed using installation packages.

Concept

If something unexpected happens to a Building Operation product, for example, the Building Operation product does not start or software files are missing, you can try to solve the problem by repairing the installation.

Concept

Depending on your needs, you can install all Building Operation products or a few products, such a single SmartStruxure server device with a connected WorkStation.

Concept

This is an additional solution instead of first manually uninstalling the current product and then installing a new copy.

Concept

To uninstall a Building Operation product you use the Windows Add Remove Program tool. The Windows Add Remove Program tool permanently removes the Building Operation product from the computer or server.

Concept

The Building Operation version number is constructed with four numbers, which represents different parts of the version: Major, Minor, Maintenance, and Build.