15 Topic(s)
Before upgrading the system, it is strongly recommended that you archive the historical data and back up the EcoStruxure BMS servers to preserve the current data and configurations. If you plan to upgrade WebReports, be sure to back up the Reports database in SQL Server.
To uninstall an EcoStruxure Building Operation product you use the Windows Add Remove Program tool. The Windows Add Remove Program tool permanently removes the EcoStruxure Building Operation product from the computer or server.
You uninstall Device Administrator to permanently remove the application from your computer.
The EcoStruxure Building Operation software version number is constructed with four numbers, which represents different parts of the version: Major, Minor, Maintenance, and Build.
Depending on your needs, you can install all EcoStruxure Building Operation products or a few products, such a single SmartX server with a connected WorkStation.
This is an additional solution instead of first manually uninstalling the current product and then installing a new copy.
You reinstall the Device Administrator to replace your current installation with a fresh copy.
You repair the Device Administrator installation if any problems are caused by the current installation.
To be able to run the EcoStruxure Building Operation software you need to install and licensing the software.