earth_america
user_standard Log on
action_search_stroke
earth_america

DO-FC-8

Refine your search
arrow2_down
Refine your search
Ok
Ok
Ok

46 Topic(s)

Hardware Installation

Part number: SXWTBIOW110002

Concept

For Central IO modules with outputs, the following components on the front provide control of the output channels:

Concept

By adding a variety of Central IO and power supply modules, you can use the AS-P server to tailor the Intelligent Building Management System to your unique requirements.

Concept

This section outlines the recommended cables and wires, specifying the appropriate wire sizes and lengths for the Central IO modules.

Concept

There are many different kinds of external devices from different vendors that can be connected to an EcoStruxure BMS.

User Interface

The Central IO modules have the following status indicator LEDs on the front of the module:

Concept

The wiring recommendations provide guidance regarding wiring of the Central IO modules, automation servers, RP and MP controllers, IP-IO and RP-IO modules, RP controller expansion modules, Operator Display, and Twisted Pair Adapter.

How to

You can wire a terminal base prior to installing an electronics module.

Concept

This section provides recommendations on minimum wire sizes (cross-sectional areas) and maximum wire lengths for the wires connected to the screw terminals of Central IO modules, AS-B servers, RP and MP controllers, and IP-IO and RP-IO I/O modules. Recommendations on minimum wire sizes and maximum cable lengths for the various inputs and outputs of the different RP controller expansion modules and the KNX Modbus gateway are also provided. The recommendations are for guidance only. Other wire sizes and lengths may be used, depending on wiring rules and when appropriate.

Concept

The terminal bases are used for SpaceLogic devices that are based on the patented two-piece design. The terminal base provides the I/O bus to the electronics module installed on the terminal base as well as to the SpaceLogic device installed to the right (next terminal base in the chain).