1278 Topic(s)
All system events, as well as information and circumstances, are recorded in the Event log. These event records can be viewed in the Events pane or in an Event View.
Use the Semantic navigator dialog box to navigate in the semantic database.
Listed below are the System Alarms with IDs that begin with the letters E-L.
When configuring the alarm, you can write a message that displays in the Alarms pane, Events pane, Alarm Views, and Event Views when an alarm is triggered or reset.
Use the Policies tab to edit the policies for the domain.
Use the Alarm State Sort Order dialog box to change the order in which alarms of different states are displayed in the Alarms pane or the Alarm Views in the EcoStruxure Building Operation software.
When configuring an alarm, you define the priority of the alarm. The priority is used to inform the operator of the importance of the triggered alarm. The priority is displayed in the Alarms pane, Events pane, Alarm Views, and Event Views.
Alarm filters are used to set up the conditions for the alarms you want to be displayed in an Alarms pane or an Alarm View. You also use alarm filters to determine the conditions that have to be met before a sum alarm is triggered, an email notification is sent, a write to file notification is written, or an alarm is automatically assigned to a user.
You can reset the administrator password on your EcoStruxure Building Operation servers if you, for example, have locked yourself out.
You create a tenant repository to limit the semantic information to a specified group of users.