48 Topic(s)
These hardening guidelines apply to the EcoStruxure Building Commission mobile application.
You engineer your system using the engineering tools.
You can select the Feedback option to rate your experiences and provide detailed information on the Commission mobile application.
SmartX Advanced Display v3 (AD v3) is the successor to AD v2. AD v3 provides an industrial grade Human Machine Interface (HMI), with battery-free power supply, for local access to the EcoStruxure BMS servers.
You can choose from several different options to connect the eCommission SmartX Controllers mobile application to one or more SmartX IP controllers.