990 Topic(s)
You import trend log data to move trend log data between systems.
Use this workflow to change the operating system on the computer where the Enterprise Server is installed. You can also use this workflow to migrate WebReports or the Enterprise Server to another computer.
You add an attachment, for example a .pdf file or trend log, to assist the user when diagnosing or solving the problem that caused an alarm.
You add an attachment, for example a .pdf file or a trend log, to assist the user when diagnosing or solving the problem that caused the alarm.
You configure an alarm to make a sound when it is triggered so that the operator can hear the alarm.
You configure the built-in Alarm pane to automatically open an Alarm View dialog box in a new window when an alarm is triggered.
You disable incoming HTTP communication to increase the data security of your system.
Values in the EcoStruxure Building Operation software are stored in the EcoStruxure Building Operation database with all input decimals. If a stored value consists of more decimals than the operating system is defined to display, the value is rounded off according to the operating system settings before it is displayed in WorkStation.
When you configure a schedule that controls events in a single part of a building, you might also want the same events to occur in other areas of the building. You can establish a lead and shadow relationship to synchronize the events in schedules and dates in calendars.
You configure a schedule as a shadow to synchronize it with a schedule that already contains all weekly events and exception events.