17 Topic(s)
To run the EcoStruxure Building Operation software, you need to install and license the software. To keep your system maintained and up to date, you need to upgrade the software.
The EcoStruxure Building Operation software version number is constructed with four numbers, which represents different parts of the version: Major, Minor, Maintenance, and Build.
When uninstalling the building management system it is also important to securly dispose the products.
You uninstall WorkStation to permanently remove the application from your computer.
You repair the WorkStation and client tools installation if any problems are caused by the current installation.
This is an additional solution instead of first manually uninstalling the current product and then installing a new copy.
You reinstall WorkStation and client tools to replace your current installation with a fresh copy.
Depending on your needs, you can install all EcoStruxure Building Operation products or a few products, such a single field server with a connected WorkStation.
You install WorkStation and client tools to create and supervise your EcoStruxure BMS.