99 Topic(s)
You wire the terminal blocks installed on the IP-IO module to connect I/O devices and power.
You remove a terminal block from an IP-IO module in order to replace the module.
Part number: SXWMPCDSP10A01
Part numbers: SXWIPIOAA10A01, SXWIPIOBA10A01, and SXWIPIOCA10A01
You install the terminal blocks on an IP-IO module to add or enable wiring for the device.
The IP-IO module has a built-in power supply designed to accommodate 24 VAC at 50/60 Hz or 24 to 30 VDC input power.
You can select the Feedback option to rate your experiences and provide detailed information on the Commission mobile application.
You install an IP-IO module on a DIN rail inside a cabinet to ensure that the device is securely fastened and to allow for sufficient ventilation.
This section provides recommendations on wire sizes and lengths for the IP-IO modules.