IP-IO

122 Topic(s)
Use the filters below to limit the number of search hits.
Functionality
Display all
Basic Functionality
Hardware
Central IO
Programming
Trends
Alarms
Schedules
Graphics
Reports
BACnet
LonWorks
Localization
License Management
Engineering
Import/Export
User Management
I/NET
MicroNet
Sigma
MNB
Modbus
Xenta
b3
NETWORK 8000
MNL
Communication Configuration
Web Services
Upgrade
Registration
Vista Transition
Security
Smoke Control
SmartDrivers
Transition
Continuum Transition
Infinet
Custom Types
BACnet/IP devices
3-button
LCD
Touchscreen
SpaceLogic Sensor Interfaces
RP Controller Expansion Modules
Engage Mobile Application
Zoning
RP-C-RC-BLE
KNX
Zigbee
IoT
SE8000/VT8000
Administration
Semantic
Information Type
Display all
Concept
User Interface
Troubleshooting
Developers Reference
Specifications
How to
Hardware Installation
Topic
Modified
Rating
Filtering the Device List
You can filter the device list to help you find a specific device or group of devices more easily.
7/23/2021
I/O Configuration Screen
Use the I/O Configuration screen to locally configure inputs and outputs, to go to the About screen or Status screen, and to exit the configuration mode.
7/23/2021
IP-IO Module Device Installation
The IP-IO module device can be installed on a DIN rail or other flat surface inside a cabinet.
7/23/2021
IP-IO Module Built-in Power Supply
The IP-IO module has a built-in power supply designed to accommodate 24 VAC at 50/60 Hz or 24 to 30 VDC input power.
7/23/2021
IP-IO Module Reset Modes
You can reset and restart the IP-IO modules in different ways depending on how long you press the reset button. The resets and restarts can affect the retention of values after restart based on the retain levels configured for the variables.
7/23/2021
IP-IO Module Supported Building Standards
One of the cornerstones of the EcoStruxure BMS is support for open standards. As a result, the IP-IO module complies with the BACnet open standard, one of the most popular standards for buildings.
7/23/2021
IP-IO Modules
The IP-IO module provides I/O expansion to your HVAC application over BACnet/IP and can share their I/O resources across applications running in automation servers, BACnet/IP controllers, or third-party systems. The IP-IO module can be installed near facilities in the field, away from the automation server or the BACnet/IP controller.
7/23/2021
Configure Inputs and Outputs for Temporary Use
In configuration mode, you can locally configure inputs and outputs for temporary use during commissioning of the device. You can configure inputs and outputs that have not been configured through WorkStation.
7/23/2021
Keys
You use the keys on the override display to navigate the screens of the user interface and to select options on menus and lists.
7/22/2021
Installing an IP-IO Module on a Flat Surface
You install an IP-IO module on a flat surface inside a cabinet to ensure that the device is securely fastened and to allow for sufficient ventilation.
7/22/2021

Product version

Language