earth_america
user_standard Log on
action_search_stroke
earth_america

IP-IO

Refine your search
arrow2_down
Refine your search
Ok
Ok
Ok

128 Topic(s)

Concept

This section provides recommendations on minimum wire sizes (cross-sectional areas) and maximum wire lengths for the wires connected to the screw terminals of Central IO modules, AS-B servers, RP and MP controllers, and IP-IO and RP-IO I/O modules. Recommendations on minimum wire size and maximum cable length for the digital inputs of the RP controller expansion modules, the DALI bus of the DALI light modules, the SMI Interface of the SMI blind modules, the Zigbee DALI and 0-10V modules, and the KNX Modbus gateway are also provided. The recommendations are for guidance only. Other wire sizes and lengths may be used, depending on wiring rules and when appropriate.

How to

You export an Asset list when you have completed the capture of controller data. 

Concept

You can use the Asset List Creator feature to capture device information contained in the digital matrix symbol on the tear-off product information label packaged with the BACnet/IP controller. When you scan the data matrix with the Commission mobile application, the Asset List Creator saves this information to a data file that can be exported and used in documenting the physical location of the controller on the job site.

How to

You can use the Asset List Creator function of the Commission mobile application to capture device information from the Digital Matrix symbol on the tear-off product info labels of BACnet/IP devices.

Concept

The IP-IO module contains a combination of Ethernet and USB communication ports.

How to

Use the Device Restart function to perform a device restart of the BACnet/IP controller.

How to

You log on to the Commission mobile application to perform commissioning, flow balance, and checkout operations on BACnet/IP controllers.

Concept

When connecting to a network at the job site, the Commission mobile application device must have either a dynamic or static IP address.

How to

You perform I/O checkout on the Multi-I/O module to verify that the devices are wired correctly and that the physical inputs and outputs are working properly.

Concept

After you have wired the physical inputs and outputs of the controller, you perform I/O checkout to verify that the wiring was done correctly and that the physical inputs and outputs are working properly.