​License Administrator

77 Topic(s)
Use the filters below to limit the number of search hits.
Functionality
Display all
Basic Functionality
Hardware
Central IO
Programming
Trends
Alarms
Schedules
Graphics
Reports
BACnet
LonWorks
Localization
License Management
Engineering
Import/Export
User Management
I/NET
MicroNet
Sigma
MNB
Modbus
Xenta
b3
NETWORK 8000
MNL
Communication Configuration
Web Services
Upgrade
Registration
Vista Transition
Security
Smoke Control
SmartDrivers
Transition
Continuum Transition
Infinet
Custom Types
BACnet/IP devices
3-button
LCD
Touchscreen
SpaceLogic Sensor Interfaces
RP Controller Expansion Modules
Engage Mobile Application
Zoning
RP-C-RC-BLE
KNX
Zigbee
IoT
SE8000/VT8000
Administration
Semantic
Information Type
Display all
Concept
User Interface
Troubleshooting
Developers Reference
Specifications
How to
Hardware Installation
Topic
Modified
Rating
Creating the Request Files
You create request files to request response files with activated licenses from License Activation Server (FNO).
7/23/2021
EcoStruxure Building Operation Software Feature License Strings
The feature strings are used when you troubleshoot a license problem. The strings are visible in the Diagnostic tab of License Administrator.
7/23/2021
EcoStruxure Building Operation Software Licensing Installation and Location
License Administrator and License Server must run on the same computer as Enterprise Server or Enterprise Central that will use the licenses.
7/23/2021
Installation Example
Schneider Electric recommends that you install the license server framework before installing other EcoStruxure Building Operation software applications and automation servers. The license server installation is included in the License Administrator license package. During the installation of WorkStation or Enterprise Server, the installation software asks for the address to the license server.
7/23/2021
Installation Overview
The EcoStruxure Building Operation software products are installed using installation packages.
7/23/2021
License Information
The License Information in the Control Panel gives you an overview of the licenses in your EcoStruxure BMS.
7/23/2021
License Settings Dialog Box
Use the License Settings dialog box to view the license setting.
7/23/2021
License Enforcement
License enforcement is the process of checking whether a software application has a valid license available to it at runtime. If you do not have enough licenses, a license violation occurs. This is accomplished by a license violation bar in WorkStation and WebStation.
7/23/2021
Demo Licensesing Overview
Demo licenses are used for demonstration purposes, training, or when building a site.
7/23/2021
Activating Licenses Online
You activate licenses so that you can access the features.
7/23/2021

Product version

Language