60 Topic(s)
You configure the address to License Server so Enterprise Server, WorkStation, or a client tool knows where to find available licenses to activate.
You create request files to get a response file with activated or returned licenses from License Activation Server.
There are a number of different clients, servers, and features that requires licenses to operate.
Device Administrator is used to manage licenses on field servers.
Licenses are needed for EcoStruxure Building Operation products and features that run on Windows.
After licenses are activated on the License Server you have to configure Workstation and its client tools connection to License Server, where licenses are available to be activated. The address to the License Server is defined during the installation of WorkStation. This is done using License Administrator.
You view all EcoStruxure Building Operation software licenses and the license details located on the License Server. This diagnostic information is helpful when you are troubleshooting.
You view all the activated EcoStruxure Building Operation software licenses on the License Server on the same computer as the License Administrator.
You upload request files to the License Activation Server (FNO) with license information so that you can receive response files that you send to the field server.