45 Topic(s)
You configure the address to License Server so Enterprise Server, WorkStation, or a client tool knows where to find available licenses to activate.
There are a number of different clients, servers, and features that requires licenses to operate.
Licenses are needed for EcoStruxure Building Operation products and features that run on Windows.
After licenses are activated on the License Server you have to configure Workstation and its client tools connection to License Server, where licenses are available to be activated. The address to the License Server is defined during the installation of WorkStation. This is done using License Administrator.
You view all EcoStruxure Building Operation software licenses and the license details located on the License Server. This diagnostic information is helpful when you are troubleshooting.
You view all the activated EcoStruxure Building Operation software licenses on the License Server on the same computer as the License Administrator.
When uninstalling the building management system it is also important to securly dispose the products.
Before upgrading the system, it is strongly recommended that you archive the historical data and back up the EcoStruxure BMS servers to preserve the current data and configurations.
You start License Administrator to administer the licenses on the License Server and define the address to the License Servers for all licensed EcoStruxure Building Operation products.