earth_america
user_standard Log on
action_search_stroke
earth_america

Mobile Apps

Engage
Commission
HMI Kiosk
SmartXKiosk
Technician Tool for iOS
Technician Tool for Android
Refine your search
arrow2_down
Refine your search
Ok
Ok
Ok

45 Topic(s)

Specifications

How to

You can select the Feedback option to rate your experiences and provide detailed information on the Commission mobile application.

Specifications

Concept

SmartX Advanced Display v3 (AD v3) is the successor to AD v2. AD v3 provides an industrial grade Human Machine Interface (HMI), with battery-free power supply, for local access to the EcoStruxure BMS servers.

Hardware Installation

Concept

You engineer your system using the engineering tools.

Concept

You can choose from several different options to connect the eCommission SmartX Controllers mobile application to one or more SmartX IP controllers.

Concept

Prior to using the eCommission SmartX Controllers mobile application at a job site, there are certain preparations that must be made. Complete the following tasks, as well as any additional tasks that may be necessary.

How to

You launch and then activate the eCommission SmartX Controllers mobile application so that it can be used.

Troubleshooting

You use the Controller List Creator function of the eCommission SmartX Controllers mobile application to scan the tear-off product info label on a SmartX IP controller. In the List Creator view, you note that the captured data appears in red text, indicating that you have duplicated a previous scan. This duplication is also indicated with red text in the originally scanned data set.