Power Supply

24 Topic(s)
Use the filters below to limit the number of search hits.
Functionality
Information Type
Topic
Modified
Rating
6/6/2019
6/6/2019
Wiring a Terminal Base
You can wire a terminal base prior to installing an electronics module.
5/22/2019
Installing a Terminal Base on a DIN-rail
You install a terminal base on a horizontal DIN-rail prior to connecting it to its neighboring terminal bases.
5/20/2019
Device Installation
The devices are designed mainly for installing on DIN rails in a cabinet.
5/20/2019
Installing an Electronics Module on a Terminal Base
You install an electronics module directly onto the relevant terminal base, where it will connect to the power supply and address bus.
5/19/2019
Connecting Terminal Bases
You connect terminal bases together to provide continuity of the power supply and the address bus.
5/4/2019
5/25/2018
Powering Up a Device
You perform the following steps to power up a device.
3/3/2018
Power Budget
Use the power budget to calculate the maximum number of devices that the power supply can supply. If more devices are used, additional power supplies must be added to the I/O bus.
10/12/2017

Product version

Language