earth_america
user_standard Log on
action_search_stroke
earth_america

Project Configuration Tool

Refine your search
arrow2_down
Refine your search
Ok
Ok
Ok

963 Topic(s)

How to

You add an attachment, for example a .pdf file or trend log, to assist the user when diagnosing or solving the problem that caused an alarm.

How to

You add an attachment, for example a .pdf file or a trend log, to assist the user when diagnosing or solving the problem that caused the alarm.

How to

You configure an alarm to make a sound when it is triggered so that the operator can hear the alarm.

How to

You configure the built-in Alarm pane to automatically open an Alarm View dialog box in a new window when an alarm is triggered.

How to

You disable incoming HTTP communication to increase the data security of your system.

Concept

​Values in the EcoStruxure Building Operation software are stored in the EcoStruxure Building Operation database with all input decimals. If a stored value consists of more decimals than the operating system is defined to display, the value is rounded off according to the operating system settings before it is displayed in WorkStation.

Concept

When you configure a schedule that controls events in a single part of a building, you might also want the same events to occur in other areas of the building. You can establish a lead and shadow relationship to synchronize the events in schedules and dates in calendars.

How to

You configure a schedule as a shadow to synchronize it with a schedule that already contains all weekly events and exception events.

How to

You configure a calendar as a shadow to synchronize it with a calendar that already contains all exception dates, date ranges, or calculated dates, such as a holiday calendar.

Specifications