earth_america
user_standard Log on
action_search_stroke
earth_america

PS-24V

Refine your search
arrow2_down
Refine your search
Ok
Ok
Ok

32 Topic(s)

Concept

PS-24V is the power supply for the AS-P servers and Central IO modules. The PS-24V power supply requires an input voltage of either 24 VAC +/–20 % or 24–30 VDC.

Specifications

Hardware Installation

Part number: SXWTBPSW110001

How to

You can wire a terminal base prior to installing an electronics module.

Hardware Installation

Part number: SXWTBPSW110002

Hardware Installation

Part number: SXWPS24VX10A01

Hardware Installation

Part number: SXWTBPSW110A01

Hardware Installation

Part number: SXWPS24VX10001

Concept

The Schneider Electric EasyLogic and SpaceLogic hardware devices for the EcoStruxure BMS include terminal bases, PS-24V power supplies, Central IO modules, automation servers such as AS-P-3, AS-P and AS-B servers, MP-C, MP-V, RP-C, and RP-V controllers, IP-IO and RP-IO I/O modules, RP controller expansion modules, remote control, KNX Modbus gateway, Bluetooth adapter, Wireless Adapter - Advanced, SpaceLogic Sensor devices, Advanced Display devices, and Operator Display devices.

Concept

The terminal bases are used for SpaceLogic devices that are based on the patented two-piece design. The terminal base provides the I/O bus to the electronics module installed on the terminal base as well as to the SpaceLogic device installed to the right (next terminal base in the chain).