264 Topic(s)
The RP-C-16A model has 16 I/O points and the controller is equipped with 30 fixed screw terminals.
The RP-C-12C model has 12 I/O points and the controller is equipped with 24 fixed screw terminals.
The RP-C-12B model has 12 I/O points and the controller is equipped with 24 fixed screw terminals.
The RP-C-12A model has 12 I/O points and the controller is equipped with 23 fixed screw terminals.
You must configure the DIP switches as part of the commissioning process for RP controllers that support MS/TP communications.
You perform the following steps to power up an RP-C 230 V controller model.
You install an RP controller expansion Insight-Sensor on an octagon junction box using the supplied mounting ring to properly fasten the Insight-Sensor to the junction box.
You install an RP controller expansion Insight-Sensor on a ceiling using the supplied mounting ring to properly fasten the Insight-Sensor on the ceiling.
You install an RP controller expansion Insight-Sensor into a dropped ceiling using the mounting springs to properly fasten the Insight-Sensor to a ceiling tile.
You connect RP controller expansion modules and multi-sensors to the RP-C room bus to provide the devices with power and communication from the RP-C controller.