RP-C

248 Topic(s)
Use the filters below to limit the number of search hits.
Functionality
Display all
Basic Functionality
Hardware
Central IO
Programming
Trends
Alarms
Schedules
Graphics
Reports
BACnet
LonWorks
Localization
License Management
Engineering
Import/Export
User Management
I/NET
MicroNet
Sigma
MNB
Modbus
Xenta
b3
NETWORK 8000
MNL
Communication Configuration
Web Services
Upgrade
Registration
Vista Transition
Security
Smoke Control
SmartDrivers
Transition
Continuum Transition
Infinet
Custom Types
BACnet/IP devices
3-button
LCD
Touchscreen
SpaceLogic Sensor Interfaces
RP Controller Expansion Modules
Engage Mobile Application
Zoning
RP-C-RC-BLE
KNX
Zigbee
IoT
SE8000/VT8000
Administration
Semantic
Information Type
Display all
Concept
User Interface
Troubleshooting
Developers Reference
Specifications
How to
Hardware Installation
Topic
Modified
Rating
KNX Modbus Gateway Device Installation
The KNX Modbus gateway (RP-C-EXT-KNX) is designed for installation on a DIN rail. The width of the device is 1 unit (18 mm or 0.7 inch).
9/1/2020
KNX Modbus Gateway LEDs
There are three LEDs on the front of the KNX Modbus gateway (RP-C-EXT-KNX) and one LED above the front. The LEDs indicate different types of status and modes.
9/1/2020
KNX Modbus Gateway Manual Operation Mode
The manual operation mode enables you to perform two types of operations:
9/1/2020
KNX Modbus Gateway Programming Mode
When the KNX Modbus gateway (RP-C-EXT-KNX) is in programming mode, you can assign an individual address to the device on the KNX bus.
9/1/2020
KNX Modbus Gateway Regulatory Compliance and Approvals
This section provides information on regulatory compliance and approvals for the KNX Modbus gateway (RP-C-EXT-KNX).
9/1/2020
KNX Modbus Gateway Screw Terminals and Connector
The KNX Modbus gateway (RP-C-EXT-KNX) is equipped with two 3-position pluggable screw terminal blocks for connection to the RP-C Modbus (RS-485) network and a 2-pole PCB connector for connection to the KNX bus.
9/1/2020
Performing a Factory Reset of the KNX Modbus Gateway
You perform a factory reset (recovery) of the KNX Modbus gateway (RP-C-EXT-KNX) to restore the device to factory default settings.
9/1/2020
Wire Sizes and Lengths for the KNX Modbus Gateway
This section provides recommendations on wire sizes and lengths for the KNX Modbus gateway (RP-C-EXT-KNX).
9/1/2020

Product version

Language