earth_america
user_standard Log on
action_search_stroke
earth_america

RP-C

Refine your search
arrow2_down
Refine your search
Ok
Ok
Ok

294 Topic(s)

Concept

The RP-C-16A model has 16 I/O points and the controller is equipped with 30 fixed screw terminals.

Concept

The RP-C-12C model has 12 I/O points and the controller is equipped with 24 fixed screw terminals.

Concept

The RP-C-12B model has 12 I/O points and the controller is equipped with 24 fixed screw terminals.

Concept

The RP-C-12A model has 12 I/O points and the controller is equipped with 23 fixed screw terminals.

Concept

You must configure the DIP switches as part of the commissioning process for the RP and MP controllers and RP-IO modules that only support BACnet MS/TP communications.

Concept

Concept

Ensuring the EcoStruxure Building Management integration is installed securely is key to the overall security envelope of the building. The following integration security configurations need to be considered to ensure the overall security meets “best practice” standards.

How to

You connect RP controller expansion modules and multi-sensors to the RP-C room bus to provide the devices with power and communication from the RP-C controller.

Concept

Use this workflow to commission one or more devices using the Zero Friction Commissioning function in the Commission mobile application. Related information can be found in the section after the flowchart.

Concept

The Insight-Sensor supports people counting through a thermal image sensor.