38 Topic(s)
The wiring recommendations provide guidance regarding wiring of the Central IO modules, automation servers, RP and MP controllers, IP-IO modules, RP controller expansion modules, and Operator Display.
You remove an external connector from an RP controller expansion module to disconnect lights, blinds, dry contact digital inputs, or AC power from the module.
You configure the address for an RP controller expansion module to give the module a unique address on the RP room bus.
RP controller expansion modules have two types of memory, flash memory and RAM.
This section provides information on regulatory compliance and approvals for the RP controller expansion light, blind, and relay modules.
There is one or more LEDs on the front panel of the RP controller expansion modules.
The RP controller expansion modules support different modes that can be used for maintenance purposes.
You perform the following steps to power up an RP controller expansion light module.
The RP controller expansion modules provide a range of devices that can be combined to form a connected room solution. The RP controller expansion modules are connected to the RP-C room bus and provide the RP-C room controllers with I/O expansion and sensors that enable lighting and blind control.
You configure an RP controller expansion module into online maintenance mode to read diagnostics from the device and to upgrade the device with new firmware.