earth_america
user_standard Log on
action_search_stroke
earth_america

RP Controller Expansion Modules

RP-C-EXT-DALI-M-PD
RP-C-EXT-DALI
RP-C-EXT-0-10V-4-PD
RP-C-EXT-0-10V-4
RP-C-EXT-BL-SMI-4-HV-PD
RP-C-EXT-BL-SMI-2-LV-PD
RP-C-EXT-BL-4-HV-PD
RP-C-EXT-BL-2-LV-PD
RP-C-EXT-REL-4
CRS-HH-REL-10
CRS-HIRG-SDL-4
RP-C-EXT-IS-BLE
RP-C-EXT-MS-BLE
RP-C-EXT-KNX
RP-C-RC-BLE
Refine your search
arrow2_down
Refine your search
Ok
Ok
Ok

144 Topic(s)

How to

You install an RP controller expansion Insight-Sensor on an octagon junction box using the supplied mounting ring to properly fasten the Insight-Sensor to the junction box.

How to

You install an RP controller expansion Insight-Sensor on a ceiling using the supplied mounting ring to properly fasten the Insight-Sensor on the ceiling.

How to

You install an RP controller expansion Insight-Sensor into a dropped ceiling using the mounting springs to properly fasten the Insight-Sensor to a ceiling tile.

How to

You connect RP controller expansion modules and multi-sensors to the RP-C room bus to provide the devices with power and communication from the RP-C controller.

Concept

The wiring recommendations provide guidance regarding wiring of the Central IO modules, automation servers, RP and MP controllers, IP-IO and RP-IO modules, RP controller expansion modules, Operator Display, and Twisted Pair Adapter.

Concept

This section provides recommendations on minimum wire sizes (cross-sectional areas) and maximum wire lengths for the wires connected to the screw terminals of Central IO modules, AS-B servers, RP and MP controllers, and IP-IO and RP-IO I/O modules. Recommendations on minimum wire sizes and maximum cable lengths for the various inputs and outputs of the different RP controller expansion modules and the KNX Modbus gateway are also provided. The recommendations are for guidance only. Other wire sizes and lengths may be used, depending on wiring rules and when appropriate.

Concept

The I/O wiring recommendations provide guidance on what type of wires should be used for the different Central IO modules, AS-B server onboard I/O, RP and MP controller onboard I/O, and IP-IO and RP-IO I/O modules, how to perform grounding, and how to connect different external devices to the inputs and outputs. This section also provides information on the external connectors required for the RP controller expansion modules and the RP-C-16C-F-230V model. Always use the recommended cables and wires.

Concept

The Schneider Electric EasyLogic and SpaceLogic hardware devices for the EcoStruxure BMS include terminal bases, PS-24V power supplies, Central IO modules, automation servers such as AS-P and AS-B servers, MP-C, MP-V, RP-C, and RP-V controllers, IP-IO and RP-IO I/O modules, RP controller expansion modules, remote control, KNX Modbus gateway, Bluetooth adapter, Wireless Adapter - Advanced, SpaceLogic Sensor devices, Advanced Display devices, and Operator Display devices.

Concept

It is important to perform the grounding correctly for the following reasons:

Hardware Installation