29 Topic(s)
The EcoStruxure Building Operation software products are installed using installation packages.
You install the Enterprise Server to collect data throughout the EcoStruxure BMS while providing supervisory control.
Depending on your needs, you can install all EcoStruxure Building Operation products or a few products, such a single automation server with a connected WorkStation.
Before upgrading the system, it is strongly recommended that you archive the historical data and back up the EcoStruxure BMS servers to preserve the current data and configurations. If you plan to upgrade WebReports, be sure to back up the Reports database in SQL Server.
Schneider Electric recommends that you install the license server framework before installing other EcoStruxure Building Operation software applications and automation servers. The license server installation is included in the License Administrator license package. During the installation of WorkStation or Enterprise Server, the installation software asks for the address to the license server.
To be able to run the EcoStruxure Building Operation software you need to install and licensing the software.
You start the server manually in case you previously have stopped it.
Use the Enterprise Server viewto start and stop the Enterprise Server service and configure the ports of the Enterprise Server.
You uninstall an Enterprise Server to permanently remove the application from your computer.
To uninstall an EcoStruxure Building Operation product you use the Windows Add Remove Program tool. The Windows Add Remove Program tool permanently removes the EcoStruxure Building Operation product from the computer or server.