earth_america
user_standard Log on
action_search_stroke
earth_america

SpaceLogic Sensor

Refine your search
arrow2_down
Refine your search
Ok
Ok
Ok

33 Topic(s)

Concept

The MP Series controller sensor bus allows SmartX Sensors to be connected to the controller.

Concept

SmartX Sensors are a family of living space sensors designed for MP Series controllers using the EcoStruxure Building Operation user interface. These sensors use an RJ-45 sensor bus that provides communication and power from the MP Series controller.

Concept

SmartX Sensors are modular and are ordered in two parts: the sensor base and the cover. Four SmartX communicating sensor base models are available as well as a variety of covers.

User Interface

Use the SmartX Sensor 3-Button Cover model interface to change the temperature setpoint to a comfortable level. You can also confirm your presence in a room and turn on the lights with the occupancy override button.

Concept

The 3-Button Cover model contains a passive, infrared sensor for occupancy detection and a plus and minus button to adjust the temperature setpoint. There is also an occupancy override button should the room occupant wish to confirm their presence, turn on the lights, and change the setpoint to a comfortable level.

User Interface

Use the SmartX Sensor LCD Temperature Sensor model Default screen to advance through the menus, increase and decrease temperature, change modes and degree types, and perform occupany overrides.

User Interface

Use the SmartX Sensor LCD Temperature Sensor model Degree Type screen to view and configure the degree type setting.

User Interface

Use the SmartX Sensor LCD Temperature Sensor model Fan Speed screen to view and configure the current fan speed.

User Interface

Use the SmartX Sensor LCD Temperature Sensor model Heating and Cooling Mode screen to view and configure the current heating or cooling setting.

User Interface

Use the SmartX Sensor LCD Temperature Sensor model Home or default screen to view the current temperature.