28 Topic(s)
You connect AD v3 to a SmartX server in order to communicate with the SmartX server over a wired (USB) connection. You connect AD v3 to a 24 VDC power supply in order to supply AD v3 with power. You use the Y-shaped cable (SXWADUSBC10002 or SXWADUSBC10003) to connect AD v3 to both the SmartX server and the power supply.
You perform a recovery (factory reset) of AD v3 to restore the device to factory default settings.
This section provides safety information specific to AD v3. Carefully read the instructions before trying to install, operate, service, or maintain the equipment.
AD v3 is installed on a control cabinet using a 22 mm (0.87 inch) cable fitting (gland) and a nut. AD v3 is delivered with the cable fitting integrated on the back cover. The position of AD v3 on the cabinet is fixed by the earth ground screw and the nut fastens the device to the cabinet.
SmartX Advanced Display v3 (AD v3) is the successor to AD v2. AD v3 provides an industrial grade Human Machine Interface (HMI), with battery-free power supply, for local access to the EcoStruxure BMS servers.
You connect AD to an Automation Server in order to communicate with EcoStruxure BMS servers over the USB connection. You connect AD to a USB power adapter in order to supply AD with power and to ensure that its battery is charged. You use a USB “Y” cable to connect AD to both an Automation Server and a USB power adapter.