earth_america
user_standard Log on
action_search_stroke
earth_america

Touch Screens

AD v1
AD v2
AD v3
Operator Display
Refine your search
arrow2_down
Refine your search
Ok
Ok
Ok

167 Topic(s)

Concept

The wiring recommendations provide guidance regarding wiring of the Central IO modules, automation servers, RP and MP controllers, IP-IO and RP-IO modules, RP controller expansion modules, Operator Display, and Twisted Pair Adapter.

Concept

The Schneider Electric EasyLogic and SpaceLogic hardware devices for the EcoStruxure BMS include terminal bases, PS-24V power supplies, Central IO modules, automation servers such as AS-P and AS-B servers, MP-C, MP-V, RP-C, and RP-V controllers, IP-IO and RP-IO I/O modules, RP controller expansion modules, remote control, KNX Modbus gateway, Bluetooth adapter, Wireless Adapter - Advanced, SpaceLogic Sensor devices, Advanced Display devices, and Operator Display devices.

Concept

It is important to perform the grounding correctly for the following reasons:

Specifications

User Interface

Use the Select a region screen to configure the time zone of Operator Display.

Concept

This section provides information on regulatory and agency compliance and approvals for the SpaceLogic Operator Display.

Concept

This section provides information on regulatory and agency compliance and approvals for the Advanced Display v3 (AD v3).

Hardware Installation

Part number: SXWADBUND10013

Hardware Installation

Part number: SXWADWIFI10002

How to

You connect AD v3 to an automation server in order to communicate with the automation server over a wired (USB) connection. You connect AD v3 to a 24 VAC or 24 VDC power supply in order to supply AD v3 with power. You use the Y-shaped cable with USB isolation (SXWADUSBC10012 or SXWADUSBC10013) to connect AD v3 to a 24 VAC power supply. You use either the Y-shaped cable with USB isolation or the Y-shaped cable without USB isolation (SXWADUSBC10002 or SXWADUSBC10003) to connect AD v3 to a 24 VDC power supply.