earth_america
user_standard Log on
action_search_stroke
earth_america

Twisted Pair Adapter

Refine your search
arrow2_down
Refine your search
Ok
Ok
Ok

19 Topic(s)

Concept

Twisted Pair Adapter supports Ethernet over twisted pair cable networks.

Concept

SpaceLogic™ Twisted Pair Adapter - Ethernet (TPA-E) connects to the SpaceLogic BACnet/IP controller and automation server via Ethernet 10/100 Mbit (IEEE 802.3) and utilizes existing twisted pair cabling originally used for legacy serial and free topology protocols. This enables seamless integration of existing twisted pair networks into the IP-based infrastructure of the EcoStruxure Building Management System (BMS), reducing installation costs and simplifying the transition from legacy systems, such as LonWorks FTT-10 networks, to the EcoStruxure BMS network.

Hardware Installation

Part number: SXWTPAE10001

Specifications

Concept

The operating modes are controlled by the M/T slide switch on the front of the adapter:

Concept

The Twisted Pair Adapter is equipped with the following connectors:

How to

You restart the Twisted Pair Adapter to intialize the device.

Concept

There are three LEDs on the front of the Twisted Pair Adapter. The LEDs indicate different types of status and modes.

Concept

The Twisted Pair Adapter supports power input from either a standard 24 VAC or 24 VDC source.

How to

You wire the screw terminals on a Twisted Pair Adapter to connect the adapter to a twisted pair cable network. Always use the recommended wires (or wires with larger cross-sectional area).