19 Topic(s)
Part number: SXWTPAE10001
Twisted Pair Adapter supports Ethernet over twisted pair cable networks.
SpaceLogic™ Twisted Pair Adapter - Ethernet (TPA-E) connects to the SpaceLogic BACnet/IP controller and automation server via Ethernet 10/100 Mbit (IEEE 802.3) and utilizes existing twisted pair cabling originally used for legacy serial and free topology protocols. This enables seamless integration of existing twisted pair networks into the IP-based infrastructure of the EcoStruxure Building Management System (BMS), reducing installation costs and simplifying the transition from legacy systems, such as LonWorks FTT-10 networks, to the EcoStruxure BMS network.
The operating modes are controlled by the M/T slide switch on the front of the adapter:
The Twisted Pair Adapter is equipped with the following connectors:
You restart the Twisted Pair Adapter to intialize the device.
There are three LEDs on the front of the Twisted Pair Adapter. The LEDs indicate different types of status and modes.
The Twisted Pair Adapter supports power input from either a standard 24 VAC or 24 VDC source.
You wire the screw terminals on a Twisted Pair Adapter to connect the adapter to a twisted pair cable network. Always use the recommended wires (or wires with larger cross-sectional area).